Hello, I have a AVR question that I have been set from my class. Please note: I AM NOT ASKING YOU TO ANSWER THE QUESTION!I m just asking to see if it correct as i have no simulation software or hardware available at the time. I have supplied my answer with workings the chip i m using is a ATMega164P
An AVR is running from an 11.0592MHz clock. For serial transmission only, at 4800 Baud:
Which bit(s) in the UCSR0B need to be set?
What value needs to be loaded into the UBRR0 register? (Assume U2X0 = 0.)
----ATMega164p----
My Answer:
From the data sheet I would set bits: 1<<TXCIEn | 1<< TXEn | 1<<TXB8n
The values that need to be loaded into the UBRR0 register are:
UBRR0 = ( f / (16XBaud Rate)) -1
UBRR0 = 143
So values 143 needs to be loaded into the register
Can someone who is familiar with micro controllers confirm my answers as I am new to this. If they are wrong could you please correct me. Much appreciated
Thanks