A little background on my project:
home made electric go kart
Motor: 48v 1000w brushed
Speed controller: 48v 1000w (x2)
Battery: homemade Lypo 12s 18A
I’m wiring my sons go kart up and have run into an issue. His go kart has no space for a mechanical brake, so I decided I would use the motor as a brake by switching the polarity of the battery. Since I have 2 of the same speed controllers I figured I would use one controller to go forward and the other for reverse/brake. I have 2 throttle levers attached to the steering wheel that are a lot like paddle shifters on a car. They are wired through the frame of the kart and are connected to their own speed controller. The positive and negative power wires are connected in parallel and connect to the battery.
And this brings me to why I’m writing this. Because I have 2 speed controllers I also have 2 outputs that are going to be connected together going into one input (motor). If I use the accelerator throttle the +48 volts will be going into the motor like it should but it will also be traveling into the reverse/brake speed controller and most likely ruining that speed controller and vise versa the -48v will travel into the accelerator speed controller.
Is there a way to completely block the voltage that would be going into the output speed controller that isn’t being used ?