Hi all!
Well, I’m now starting to play with Bluetooth, or BlueTeeth since I have 2 modules (
)…
There are 18 pins off this eval board, but only 7 are labeled, does anyone know what the others are? I’m assuming thet are the pio pins?
Thanks!
~Kam (^8*
Well, looking at the spec, and using my eyeballs, here are the mappings
These are the DIP mappings, DOUBLE CHECK BEFORE USING, WOULD HATE TO BLOW YOUR DIP UP!
Pin 1: Ground
Pin 2: SPI_MOSI
Pin 3: RESET
Pin 4: SPI_CLK
Pin 5: PCM_CLK
Pin 6: PCM_SYNC
Pin 7: PCM_IN
Pin 8: PCM_OUT
Pin 9: VDD (3.3v)
Pin 10: UART_RX
Pin 11: UART_TX
Pin 12: UART_RTS
Pin 13: UART_CS
Pin 14: PIO(2)
Pin 15: PIO(5)
Pin 16: PIO(4) ← apply 3.3v for >2 sec for complete system reset!
Pin 17: SPI_CSB
Pin 18: SPI_MISO
Again, double check “just in case”…standard warrantees apply…bla bla bla
~Kam (^8*