Hello,
I’ve a problem that make me mad ![]()
I’ve bought a BlueSMIRF-RPSMA to connect to my RP6 Robot (ATMEGA32).
On the microprocessor i loaded a question and answer program that works perfectly if the micro is connected via real serial interface.
The BT creates the com port and i can connect the device and receive on the pc terminal it’s output but my answers seems to be ignored. It seems that just the connection from (and not to) the microprocessor works.
The connections seems to be right: Rx and Tx are inverted and cts-rts pins are connected togheter.
Someone has the same problem or is there any Bluesmirf setting i miss to resolve this one-way communication problem?
Thanks a lot / Francesco