Hello all,
I successfully connected my BlueSmirf Gold module to my Mac and can send commands to it.
The status of the module is as follows:
D
***Settings***
BTA=00066600D32A
BTName=FireFly-D32A
Baudrt(SW4)=115K
Parity=None
Mode =Mstr
Authen=1
Encryp=0
PinCod=0000
Bonded=0
Rem=001C4D30FB99
E
***ADVANCED Settings***
SrvName= SPP
SrvClass=0000
DevClass=1F00
InqWindw=0200
PagWindw=0200
CfgTimer=60
StatuStr=NULL
When I start an Inquiry this works fine, but I can’t connect to the device since the device I want to connect to will request a PIN to pair/connect.
I can inquire using the “I” command:
I
Inquiry, COD=0
Found 1
001C4D30FB99,Zeemote JS1,584
Inquiry Done
and after I try to connect this fails.
C,001c4d30fb99
TRYING
CONNECT failed
How can I connect/pair using a pin which is requested by the client device?
The Pin is just “0000” but where and how do I specify that?
Thank you very much in advance,
Michael.