No PIN request on connect?

I’ve used the BleuSmirf with the Pin code set as ‘default’, but recently I noticed I was able to connect a new (not used to connect to the smirf before) laptop without it asking for a password…

I changed the pin code with the ATSP command, and also checked the security level (set to ‘0’ Link level).

I am still able to connect to the smirf without entering a password…

I did a reset (power cycle of the module), removed the BT connections from the pc(s), but still it allows anyone to connect without asking for a password…

I am missing something here?

I don’t want to enter the pin every time with the AT command, but I assume that it should ask for the password while pairing devices?

Any ideas?

Thanks

Always helps when you write …

Used the ATCPAIR command to delete the excisting paired devices, and that worked. after removing and installing the device again on the pc(s) it asked for the correct password…