BlueSMiRF up, but not communicating

So, here’s the drill. I’ve got a BlueSMiRF connected very simply to a BasicStamp 2. I’ve got the pin that is transmitting serial data connected to RX of the BlueSMiRF. I’m able to connect to the BlueSMiRF from another computer, using Bluetooth, to get the BlueSMiRF’s ATtention and such all, no problem.

When I connect ZTerm or run screen from my machine to connect to the BlueSMiRF, the connection is established (I can get AT and the red LED on the BlueSMiRF illuminates), but no data is sent.

My suspicion is that there was a mismatch between the BlueSMiRFs baud rate and the one I was using in the program, but I’ve tried various rates and, until I get the AT Command Ref for the BlueSMiRF, I’m just guessing this is the problem.

Has anyone else seen this, or know what the mystery might be?

Julian