Hi,
I have a https://www.sparkfun.com/commerce/produ … ts_id=8550 and this are the Settings
BTA=000666014CC6
BTName=CCPC
Baudrt=9600
Parity=None
Mode =Slav
Authen=0
Encryp=0
PinCod=1234
Bonded=0
Rem=000B0D098086
I have use a Logic Level Converter and a PIC 16f877a (5v) this is my wardware setup.
This is a simple code in PBP to see if pic is talking to the BT
@ Device HS_OSC
define OSC 20
Include “modedefs.bas” ’ Include serial modes
TrisB.5=1 ’ Rx BT
TrisB.4=0 ’ Tx BT
TrisB.0=0
Pause 5000
Serout2 Portb.4,84, [“$$$”,13]
Pause 5000
Serin2 Portb.5,84, [wait(“CMD”)]
High PortB.0
End
Using the a PC USB BT to config. the module i can comunicate very well with the module send “$$$” and received “CMD” more and more …
And my big big problem is when using the pic to config. the module the led dont light, i tryed connecting the BT with a PC USB BT and the pic at same time and using hyperterminal to see what is going on and i saw the “$$$” send by the pic but not the response from rthe BT “CMD”.
Can you people hellp me?
Thanks for caring.](http://imageshack.us)