BlueTooth DIP Module WRL-08469 not responding

Hi,

I just got my BlueTooth DIP Module WRL-08469.

The blasted thing does not respond at all when my PIC, a Propeller (it’s a 3v microcontroller) sends it commands.

I have tried +++, AT, ATI, and so on. Nothing makes it respond.

I just want to use the TX and RX to control it so I have CTS/RTS jumpered together, and Tx and Rx setup. (even tried reversing tx/rx in case that was it) at 115200 baud.

The documentation I have is:

UM_1SPP BGB203 BT 2.0 Serial Port Profile Module User’s Guide

Rev. 1.0.3 — 21 December 2005

I can ‘see’ it with my BT Terminal app and connect to it easily. But that’s it.

Arrrg.

Any help would be greatly appreciated!

Thanks,

Joe

edited: more detail was added

Ok, so the doc says the default baud is 155200.

It’s not, its 9600.

works now.

Thanks anyhow :slight_smile:

Yes. I caught it later. SF has programmed the modules so the module that you receive from SF is not programmed w/ ‘factory defaults’. From the product description:

We have pre-programmed these units with a unique MAC address, unit name of ‘SparkFun-BT’, and a UART interface of 9600bps.

Good luck,

John