I don’t know if anyone on here is familiar with the Turtle Beach XBA, but it is a bluetooth adapter that was designed for the Xbox 360 and to allow the user to use a bluetooth headset when the adapter was plugged into the 2.5 mm headset port on the controller.
What I want to do is develop a similar adapter from scratch. If anyone wants to help me with this project, please let me know. I would appreciate all the help I can get. Here are a few pictures of the XBA out of its housing and the 2.5 mm male plug removed.
http://i916.photobucket.com/albums/ad1/ … G_5574.jpg http://i916.photobucket.com/albums/ad1/ … G_5577.jpg http://i916.photobucket.com/albums/ad1/ … G_5575.jpgThanks