BME690 Development Kit

BME690 will supercede BME688. Is there any possibility that a BME690 Development Kit is on the horizon? The Bosche BME690 offering (Shuttle Board and Application Board) is not a like-for-like replacement of the BME688 Development Kit and costs much more.

I’d guess it’s 50/50, but we don’t have any insider info…we’ve been carrying that line for a long time and we currently carry 3 versions of their BME, if we were to add the 690 I’d presume we’d try to phase one out…

Scroll down to the bottom of any sparkfun.com page and you can sign up for the newsletter in the bottom right of the page to be alerted if/when!

Hi,

Thanks for your note. For the moment I will just wait and keep my fingers crossed.

BTW is it possible to commission a product from Sparkfun. I would obviously be incurring a much higher cost but it may be worthwhile to ger my hands on a BME690 Development Kit sooner rather than later.

Geoff

Not currently (except for LARGE orders); but you can order some here Gas sensor BME690 | Bosch Sensortec and then using the datasheet you could order some pre-fab PCBs from some place like jlcpcb and re-flow the sensors onto a board you’ve designed (it looks like i2c and SPI are available as communication protocols)

Hi,

I have just spoken with jtcpcb and they suggested: kindly ask Sparkfun for the gerber file, Bill of materials and the CPL file for the components in the board. This was in response to my enquiry about creating a BME690 version of the BME688 Development Kit.

Can you release these files to me, or pass them onto jctpcb on my behalf.

Geoff

It doesn’t look like sparkfun has those files. It would take an engineer somewhat considerable time to make a design then create the files needed to manufacture a board.

Unfortunately you would need to do the design first then send the files to jlpcb. Only then could the make the actual board for you.

Maybe Bosch could provide you a copy of their files for the older dev kit and you could modify them for the BME690?

I can’t speak for sparkfun but doubt they have the time and manpower to do a one off board for you. If you’re not able to design it on your own you might find an EE freelancer that can do it for you.

I don’t see there being enough demand for something like this for SFE to put the money and effort required to make it.

Hi,

I am grateful for your comments and will follow up on your suggestion to contact Bosche Sensortec.

Geoff

The application board 3.1 contains a microcontroller (Arm Cortex M4) so it replaces the Huzza32, and the shuttle board collection included single and 8x BME690 sensors. So it provides a standard in-house dev platform. If like me you are not on Arduino then the BME690 shuttle board can be used without the Appboard using the I2C or SPI pins, the main issue is the narrow pitch, but a couple of mounts and a piece of plastic later I had created something to hook up to a PI I2C. Pimoroni have a new 690 module available, and I see Bosch say do not use BME680 in new projects. The 8x 690 shuttle board is hard to get hold of, and that’s needed for data collection/AI model generation.

can you please provide a link to the The 8x 690 shuttle board?

Also has anyone made any progress on getting that 8x shuttle board?

Here is the Sensortec 8x flyer Flyer (pdf)

There is no progress, none of the distributers Bosch list have this in stock. My guess is that it is too low volume, which is unfortunate.

Regards
Keith