Are the BoMs really the same, except for the regulator itself?
-marc
Are the BoMs really the same, except for the regulator itself?
-marc
I should probably clarify…
Ordered one 3.3vdc and one 5.0vdc breadboard power supply. I know from the product description that the boards will both have 5vdc on the silkscreen – no problem. But the resistors/capacitors for both boards are also the same – although the regulator is different (one 7805 on LM317T).
Is this just a clever design where the LM317T’s variable output is pegged at 3.3vdc based on the resitor/capacitor network and they just happen to be adequate for the 7805’s needs too?
-marc
I didn’t design that board, but we don’t normally use LM317’s for regulating. Where did you see that? I can’t find that part number in the description.
Pete
I like those breadboard power supplies; they’re pretty cool. I have a similar one that came with an electronics book.
Any chance on making one that’s switchable between 5V and 3V? Or throwing a pot on there to make it adjustable?
Mike
Pete-O:
I didn’t design that board, but we don’t normally use LM317’s for regulating. Where did you see that? I can’t find that part number in the description.Pete
The part number isn’t on the description. It’s on the regulator. I have what are supposedly one 3.3vdc and one 5.0vdc unit that I recently ordered and am trying to establish I’ve been misshipped two 5.0vdc units before I build.
The LM317T is variable output, and can actually do both output voltages.
-marc
Hummm, ok well is your bare pcb the same as the one online?
If so there are no resistors to make the referance voltage so i would not have expected the 317 to be used!
Further more with the low end power supply (6V) and the series diode (0.7V drop) u get 5.3V the lm317 i think needs about 1.2V above output to work efficiently.
So using the lm317 should only be with 3.3V applications! I would expect a low drop out variant of the 7805 for the 5V type as its much cheaper.
Just had a look on the sparkfun shopping store and have found they have the LM7805 and LM7833, 5V and 3V regulators.
With my earlier comment, the LM7805 should have a 2V drop out, so supply should be >7V…
The 3.3V one is 2V too making a minimum input voltage of 5.3V
As a follow-up: I followed the traces on the board and nothing is connected to the centre pin – therefore no reference voltage. So this definitely is a fulfillment problem.
-marc
Ok, so there is the possibilty sparkfun sent a LM317 instead of the LM7833 or LM7805
Or whoever does their fulfillment. It’s also quite easy to mistake one regulator for another ![]()
The PCB is the bit that’s important to me – I can replace the regulator with one bought at my local electronics store.
But if someone from Sparkfun can investigate, it might stop others getitng a regulator that will only generate 1.25vdc ![]()
-marc
Hey Guys!
:oops:
Please email Jeff at fun @ sparkfun.com and call him many icky names. He stuffed the kits with the wrong regulator. We’d be happy to send you a free LM7833 regulator.
The 5V kits are correct.
The 3.3V kits were shipped with the wrong regulator up until I noticed them on the 15th or 16th (last week).
Really really sorry,
-Nathan
PS - Where do we find customers like you guys?! Any other customers at any other company would be calling and yelling at us. You guys sit down and have a discussion about PCB traces and the inner-karma of a variable LM317 regulator! Thanks so much!
Heh…the reason we like Sparkfun is the curious minds we have ![]()
As a follow-up: Sparkfun added a free LM7833 to my recent order to rectify the problem and apologized for the error in an email and got a free LM317T to boot. Satisfactory end to a bit of a saga.
Oh, and Nathan confirmed that indeed the BoM for both the 5.0vdc and 3.3vdc breadboard power supply kits is indeed the same apart from the regulator itself.
-marc