I am designing a PCB that will contain a PIC microcontroller and an XBee module. Both components will normally run off of 3.3VDC, but the PIC is driven to 5VDC when I do in-circuit programming. Is this going to be an issue for the XBee module? Thanks!
According to the documents the XBee’s MAX voltage is 3.6V. So 5V would be a problem.
What I do is isolate the Vcc pin on the PIC from the system Vcc with a Schottky diode and have the ISP header connected directly to the PIC Vcc pin. This way the programmer only powers the PIC and not any other circuit.
Now no worries.
Thanks for the reply. A couple of questions:
- 
Why not a standard diode? 
- 
Should I worry about isolating the data pins between the module and the PIC? 
MagicSmoke:
- Why not a standard diode?
Good question. My reason is a Schottky has less voltage drop when conducting, ~0.4V vs 0.7V of a silicon diode at rated current.
The disadvantage of using a diode is the the PIC’s Vcc when be about 0.4 volts less than the system Vcc. For a sytem of +3.3V the PIC will be at +2.9V.
If this is unacceptable then a jumper could be used instead of a diode.
You only need to worry about the pins connected to the ISP. If these pins are normally used then the devices they connect to should be protected.
I’ve used two 4001 diodes in series
Guys, I’m curious: why isn’t the programmer powered from the target? What programmer are you using? The ISP programmer I use gets its power from the target, and hence doesn’t have these issues…
Another good question.
I use the PICStart programmer which expects the chip to be inserted into the ZIP socket so it supplies all the voltages.
For ICSP I made a cable with a DIP header that goes in the ZIP socket on the PICStart to pick-up the programing pins for the particular PIC. The other end is a 5-pin single row plug that mates with a header on the boards I build.
Maybe this is cheating but it sure beats popping the PIC out of a socket each time I wish to re-program. And I’m using the programmer I already have and works seamlessly with MPLAB.