Hello,
I’m building a Tsunami Super WAV Trigger into an enclosure to be used for an art installation. It will be playing on a continuous loop for days and I expect it will just do its job most of the time. But I’d like others to be able to stop and start it if necessary.
I would like to add some status indicators on the outside of the enclosure. I don’t believe there are any breakout pins for the status LED and I’m not prepared to or skilled enough to use the surface mount pads to achieve this.
As an alternative, I see that there is a ‘playing’ breakout pin which I believe sends a high (3.3V) signal when the device is playing.
Is this pin able to drive an LED (20mA)?
And, of course, if there are breakout pins for the status LED that I’m just not aware of, I’d be excited to know about it.
Thank you,
Michael