jremington:
In this case the Bluetooth is a slave and I2C (instead of the UART) is used by a processor to send and receive Bluetooth transmissions.
You also need a processor to read a sensor, format and send the data to the Bluetooth module.
Got it, thank you! So it doesn’t seem like there’s any options for a bluetooth board like this that are a I2C master device, everything I see either doesn’t support I2C or its a slave like this one. It would be great to find a board that didnt require a processor to function and instead can be used by itself with sensors, and have the phone basically act as the processor. I figure there has to be some, where could I find something like that?
Why? Processors are dirt cheap. Even a six pin PIC10F200 processor can do everything that is required to handle a typical dumb sensor, for $0.31.
So why should the sensor be smart? Furthermore, if your design requirements change, standard processors are reprogrammable in place, using mature, standard, freely available development software.
Perhaps you are looking in the wrong place. There are bluetooth modules with built in Arduino compatible processors, for example.
You can always use a SOC that has both a radio and Bluetooth (nRF52832, EFR32 or ESP32 comes to mind) but that will be much more work than a small micro that acts as an i2c master.
Processor + bluetooth (+WiFi & NFC if that’s of interest to you) and it’s got two I2C ports to talk to your sensor AND it’s cheaper than the bluetooth module you linked above.