Bridging BlueRadios and I2C

Alright, so I have my BlueTooth (BRSC30-A) serial device, I can communicate with it as standard serial or using AT commands. How might I go about briding the bluetooth device to an I2C bus? Is it at all possible to do such a thing with the BRSC30 without having another PIC around as a converter?

[edit]

Say possibly being able to work with the firmware on the chip to set lines 6, 7 to run the clock and the data lines?

[/edit]

[edit2]

http://www.csr.com/development/casira.htm

There are development kits out there for working with the firmware on chips like the Cambridge Silicon Radio Bluecore 2. They have the same form factor as the Bluradio’s device, but that doesn’t mean anything.

I’ll go bug MIT media labs about thier work with Bluetooth, wish me luck in finding a sympathetic ear. Or even more luck for maybe finding a solution.

[/edit2]