Hi My friends
I’m newbie with AVR U Controllers and I’m have Arduino uno and an AVR UController ATMEGA8A and using Atmel studio 7 for my code,
I’ve built IR remote control receiver with arduino uno with the help of IR library and it works very fine,
but also i want to build the same project with ATMEGA8A and using arduino library (IRRemote.h) that i’ve used befor
, so when i compile the program with the name main.c ,I’ve got a tons of error and after googling the issue i have renamed the “main.c” to “main.cpp” and compiled the app I’ve stuck with two errors
Error recipe for target ‘RemoteCtrl.elf’ failed RemoteCtrl E:\Projects\ATMEL UController\RemoteCtrl\Debug\Makefile 96 Build
Error ld returned 1 exit status RemoteCtrl collect2.exe 0 Build
Pls if any one can help
My Code
#define recvPin 0
#define outPutPin1 1
#define outPutOin2 2
#include
#include
#include "IRHeaders/IRremote.h"
int main(void)
{
DDRC=0b00000110; //DDRC=(1<<2|1<<1|1<<0);
IRrecv irrRecv(recvPin);
decode_results results;
irrRecv.enableIRIn();
while (1)
{
if(irrRecv.decode(&results) )
{
switch(results.value)
{
case 0xFD00FF:
// the required action 1
break;
case 0xFD807F:
// the required action 2
break;
}
irrRecv.resume();
}
}
}