I purchased the “LuMini LED Ring - 1 Inch (20 x APA102-2020)” and for some reason I can’t get it working.
I soldered wires to the 5V, GND, DI, & CI and attached them to an arduino mega approately (DI to PIN 16 and CI to PIN 17).
I downloaded the FastLED.h library and uploaded the “Example1_RingTest” that is provided. In the example code I defined the number of LED’s as 20 and commented the line for the 3" ring and uploaded it successfully.
Nothing happened.
I tried this on a Uno as well and a Teensy 3.2, still no luck.
Any advice on just getting it to turn on all white? nothing fancy.
Hi pfoster.
Couple questions for you. 
- Is nothing lighting up at all on the LEDs when you run that sketch?
- When you move from board to board, are you changing the clock and data pins to match what's available on your board? - Can you send pictures of the back of the LED ring and a picture showing how it's connected to your Arduino?
TS-Chris:
Hi pfoster.
Couple questions for you. 
- Is nothing lighting up at all on the LEDs when you run that sketch?
- When you move from board to board, are you changing the clock and data pins to match what's available on your board? - Can you send pictures of the back of the LED ring and a picture showing how it's connected to your Arduino?
Nothing is lighting up at all.
I do change the Data and clock pins. The Mega and the Uno are both on 16 and 17 and the Teensy 3.2 im using 18 and 19.
See picture: https://imgur.com/a/ZcPFc79
I made sure that the each pad is isolated
Thank you!
-Patrick
OK, lets try the code below with an Arduino Uno and the following wiring:
Lumini → Arduino – Your wire color
=============================
G → GND – Black
5V → 5V – Green
DI → D2 – Yellow
CI → D3 – Red
#include <FastLED.h>
#define NUM_LEDS 20 //1 Inch
// The LuMini rings need two data pins connected
#define DATA_PIN 2
#define CLOCK_PIN 3
// Define the array of leds
CRGB ring[NUM_LEDS];
void fadeAll(uint8_t scale = 250)
{
for (int i = 0; i < NUM_LEDS; i++)
{
ring[i].nscale8(scale);
}
}
void setup() {
LEDS.addLeds<APA102, DATA_PIN, CLOCK_PIN, BGR>(ring, NUM_LEDS);
LEDS.setBrightness(32);
}
void loop() {
static uint8_t hue = 0;
//Rotate around the circle
for (int i = 0; i < NUM_LEDS; i++) {
// Set the i'th led to the current hue
ring[i] = CHSV(hue++, 150, 255); //display the current hue, then increment it.
// Show the leds
FastLED.show();
fadeAll();//Reduce the brightness of all LEDs so our LED's fade off with every frame.
// Wait a little bit before we loop around and do it again
delay(50);
}
}
Give this a try with the code above (select all, copy, paste in Arduino) and let me know if the LEDs light.
If they don’t, send a photo showing the ring connected to your Arduino Uno.
TS-Chris:
OK, lets try the code below with an Arduino Uno and the following wiring:
Lumini → Arduino – Your wire color
=============================
G → GND – Black
5V → 5V – Green
DI → D2 – Yellow
CI → D3 – Red
Give this a try with the code above (select all, copy, paste in Arduino) and let me know if the LEDs light.
If they don’t, send a photo showing the ring connected to your Arduino Uno.
I don’t know what sorcery happened, but it works! Thanks you!!!