Changing BAUD rate of receiver

I have got 2 XBee XB24-DKS modules and I am trying to interface them with an on going project which I was using Bluetooth with. The problem is that the system uses 9600 and the XBee module is running at 19200 and is not compatable.

It is impossible to change the system so I need to change the BAUD rate of the receiver instead. Is this possible? And if so how can it be achieved?

Thank you

You should be able to connect to it using the X-CTU software (available for download from Digi), if you connect rx, tx, and Vss. There’s a setting for baud rate there.