changing baud rate on OpenLog with Arduino

I am new to Openlog and am using an older firmware version (1.5). I’m interfacing it with Arduino Duemilanov.

The Openlog device I’m using enters command mode with just ONE Ctrl+z and doesn’t have the CONFIG.txt feature to change the default settings.

I was trying to change the baud rate of the Openlog from the default to 57600 through Arduino but it hasn’t been working.

The code I wrote is below.

I’d appreciate any suggestions/help. Thanks.

#include <NewSoftSerial.h>
#define RXPIN 2
#define TXPIN 3

NewSoftSerial mySerial(RXPIN,TXPIN); //where OpenLog is connected

void configure_OpenLog(int baud) {
  if (baud == 9600) {
    return;
  }
  mySerial.print(26, BYTE);
  mySerial.print(13, BYTE);

  mySerial.print("baud ");
  mySerial.println(baud);
}


void setup() {
  pinMode(RXPIN, INPUT);
  pinMode(TXPIN, OUTPUT);
  pinMode(13, OUTPUT);

  mySerial.begin(9600);

  configure_OpenLog(57600);
  

}

void loop() {
  //Blink LED when done
  digitalWrite(13, HIGH);
  delay(500);
  digitalWrite(13, LOW);
  delay(500);

}