I bought two Pulse Oximeter and Heart Rate Sensors - MAX30101 & MAX32664 and I want to connect them both to one RedBoard Plus. They both work perfectly on their own.
I cut the I2C jumper trace in one of them thinking this would change the I2C address. But… after testing and verifying with a multimeter that the trace was broken, I realized they both are still at the same address.
Now I’m not sure if that jumper is in fact for changing the address or if it has a different functionality. If that is the case, can someone please explain what that jumper is for?
Do I need to get something like an I2C MUX to connect the two of them, or is there another way? Am I doing something wrong? I really thought the jumper was for changing the address. ![]()