Cirrus EP9301 EP9302

Hi,

Is there anybody whoe knows where to get Cirrus EP9301 or EP9302 in small quantities ? Farnell or Digikey do not sell them.

Marcel

it looks like newark sell them individually

http://www.newark.com/NewarkWebCommerce … &x=17&y=10

Thanks for the reply, unfortunately this is the EP73xx which is ARM7, I am looking for the EP93xx which is ARM9 and faster.

Regards,

Marcel

oh sorry i must have got my links mixed up :oops:

I recently purchased EP9301 and EP9315 from Nu Horizons, and EP7312 from Ensphere Electronics.

http://www.nuhorizons.com/

http://www.ensphereelectronics.com/

Sure would be nice if olimex did some dev boards for Cirrus Logic ARM. All of these chips have onboard audio. The EP9315 has a boatload of features including up to 6 channels audio, and IDE controller onboard.

Another ARM with audio that would be nice is Sharp LH79524/LH79525.