Cirrus EP93xx questions

I’m starting this thread about the Cirrus EP93xx questions which seem to be plentiful in these forums.

(1) It doesn’t really come with a compactflash connector does it? It comes with an SD/MMC connector, the title says CF in olimex.com and as descriptions by some redistributors.

(2) Is it possible to have a VGA DB-15 connection with the board? The EP9315 board comes with a VGA connector but I’m not sure if they use an extra chip. The datasheets didn’t look like this chip can do analog DB-15 VGA.

(3) Can the chip be clocked under 183MHz? I understand there are SDRAM timing issues but can it do say 100MHz? Can it go lower if SRAM is used? Datasheets do not explain this.

(4) What fabrication process has been used to make the chip? 0.25um? 0.13?

(5) Olimex, can you please give us a new ETA for the EP9315 board? I’m close to giving up and buying an EP9302 board and bit-banging the LCD.