How to start working with Olimex EP9302?

Am a newbie to Olimex EP9302 i dont know how to work with the board.Anyone please help me??

Am using serial cross over cable with olimex arm usb ocd Jtag .

when i connected it to hyper terminal with 57600 as BR and 8N1 and no flow control.

but am not able to see anything in the hyper terminal.

At first the green and red led’s blink at different rates.

after some time the Red with stop blinking and green continues blinking…

can anyone help me.

Awaiting anyones reply.

I strangely recall reading that the interface used 115K Baud 8N1. Give that a go.

Now the board is working with the precompiles linux kernel2.6.

the problem is with the power supply i have cjanged it to 1 A.the it worked perfectly.

Did anyone know how to connect it with eclipse and debug my program ,i am using arm usb ocd for debugging.

Thanks for the replies

Hi all,

I’m a newbie to olimex ep9302 too. I have developed several projects with microchip pic 16 & 18 series. I decided to have a begining to embeded world and i chose olimex ep9302. I’m planning to use eclipse inorder to develop projects, so i installed the everything on cd that comes with the board. However, in the documents that comes with the board there are sample programs about philips LPC2000 but i have cirrus ep9302. I need useful documents or useful sample programs like basic led application. Could u help me please? Moreover, do u have good suggestions for newbies?

Thanks in advance…

still also am not able to bring up the board.only the pre- compiles are working and i have created some linux applications and cross compiled it in windows pc using arm-elf-gcc and run that in the board and it worked perfectly.

but i am not able to port a RTOS or simple application program with the board.

if u find any program please let me know

Regards :frowning: