Quickly, here’s my set up. This is part of an interactive for children. When it works it works great.
Arduino Pro Mini (5v) hooked up to an Adafruit color sensor and a Neopixel Ring. I’ve posted this on the Adafruit forum and the admin seems to think it’s an Arduino Pro Mini issue.
There’s 10 of them all drawing 5v in parallel from a Meanwell 5v18a power supply. This is plugged into a surge protector.
I have this setup x4 so basically there’s 40 of these going.
The concept is you place a colored piece of paper in front of the sensor and as long as that paper is there the Neopixel stays that color.
Overnight the power supply is unplugged then runs for around 10 hours the next day.
Everything runs fine except periodically the arduino will just stop responding and the neopixel is unlit. The reset button does nothing, power cycling does nothing. If I re-upload the code to the arduino pro it will work fine again, almost like the code is getting corrupted somehow? Out of the 40 units it has happened 6 times over the last 4 months.
Any clue what could be going on here? I’m at a complete loss and in a situation where I can’t keep reloading the sketch every time this happens. I’ve been banging my head against the wall for weeks. ![]()
ANY HELP ON THIS IS GREATLY APPRECIATED!!!
#include <Wire.h>
#include "Adafruit_TCS34725.h"
#include <Adafruit_NeoPixel.h>
#include "Flora_Pianoglove.h"
// our RGB -> eye-recognized gamma color
byte gammatable[256];
// color sensor
Adafruit_TCS34725 tcs = Adafruit_TCS34725(TCS34725_INTEGRATIONTIME_2_4MS, TCS34725_GAIN_4X); // integreation times can be 2_4MS, 24MS, 50MS, 101MS, 154MS, 700MS -gain can be 1X, 4X, 16X, 60X
// 24 pixels on pin 6
Adafruit_NeoPixel strip = Adafruit_NeoPixel(24, 6, NEO_GRB + NEO_KHZ800);
void setup() {
strip.begin();
strip.show();
if (tcs.begin()) {
Serial.println("Found sensor");
{
for(int i = 0; i < 25 ; i++)
strip.setPixelColor(i, strip.Color(10, 80, 10));
strip.show();
delay(2000);
}
} else {
{
for(int i = 0; i < 25 ; i++)
strip.setPixelColor(i, strip.Color(100, 10, 0));
strip.show();
}
Serial.println("No TCS34725 found ... check your connections");
while (1); // halt!
}
// thanks PhilB for this gamma table!
// it helps convert RGB colors to what humans see
for (int i=0; i<256; i++) {
float x = i;
x /= 255;
x = pow(x, 3.3); //WAS 3.3
x *= 255;
gammatable[i] = x;
Serial.println(gammatable[i]);
}
}
void loop() {
uint16_t clear, red, green, blue;
delay(80); // takes 50ms to read
tcs.getRawData(&red, &green, &blue, &clear);
delay(40);
// Figure out some basic hex code for visualization
uint32_t
sum = red;
sum += green;
sum += blue;
sum = clear;
float r, g, b;
r = red; r /= sum;
g = green; g /= sum;
b = blue; b /= sum;
r *= 620; g *= 555; b *= 510; //HERE IS WHERE WE LIVE NOW WAS 255, 240, 220
if (r > 255) r = 255;
if (g > 255) g = 255;
if (b > 255) b = 255;
// OK we have to find the two primary colors
// check if blue is smallest. MEME: fix for 'white'
float remove, normalize;
if ((b < g) && (b < r)) {
remove = b;
normalize = max(r-b, g-b);
} else if ((g < b) && (g < r)) {
remove = g;
normalize = max(r-g, b-g);
} else {
remove = r;
normalize = max(b-r, g-r);
}
// get rid of minority report
float rednorm = r - remove;
float greennorm = g - remove;
float bluenorm = b - remove;
// now normalize for the highest number
rednorm /= normalize;
greennorm /= normalize;
bluenorm /= normalize;
for(int i = 0; i < 25 ; i++)
{
strip.setPixelColor(i, strip.Color(gammatable[(int)r], gammatable[(int)g], gammatable[(int)b]));
}
strip.show();
delay(20);
}
RgbColor HsvToRgb(HsvColor hsv)
{
RgbColor rgb;
unsigned char region, remainder, p, q, t;
if (hsv.s == 0)
{
rgb.r = hsv.v;
rgb.g = hsv.v;
rgb.b = hsv.v;
return rgb;
}
region = hsv.h / 43;
remainder = (hsv.h - (region * 43)) * 6;
p = (hsv.v * (255 - hsv.s)) >> 8;
q = (hsv.v * (255 - ((hsv.s * remainder) >> 8))) >> 8;
t = (hsv.v * (255 - ((hsv.s * (255 - remainder)) >> 8))) >> 8;
switch (region)
{
case 0:
rgb.r = hsv.v; rgb.g = t; rgb.b = p;
break;
case 1:
rgb.r = q; rgb.g = hsv.v; rgb.b = p;
break;
case 2:
rgb.r = p; rgb.g = hsv.v; rgb.b = t;
break;
case 3:
rgb.r = p; rgb.g = q; rgb.b = hsv.v;
break;
case 4:
rgb.r = t; rgb.g = p; rgb.b = hsv.v;
break;
default:
rgb.r = hsv.v; rgb.g = p; rgb.b = q;
break;
}
return rgb;
}
HsvColor RgbToHsv(RgbColor rgb)
{
HsvColor hsv;
unsigned char rgbMin, rgbMax;
rgbMin = rgb.r < rgb.g ? (rgb.r < rgb.b ? rgb.r : rgb.b) : (rgb.g < rgb.b ? rgb.g : rgb.b);
rgbMax = rgb.r > rgb.g ? (rgb.r > rgb.b ? rgb.r : rgb.b) : (rgb.g > rgb.b ? rgb.g : rgb.b);
hsv.v = rgbMax;
if (hsv.v == 0)
{
hsv.h = 0;
hsv.s = 0;
return hsv;
}
hsv.s = 255 * long(rgbMax - rgbMin) / hsv.v;
if (hsv.s == 0)
{
hsv.h = 0;
return hsv;
}
if (rgbMax == rgb.r)
hsv.h = 0 + 43 * (rgb.g - rgb.b) / (rgbMax - rgbMin);
else if (rgbMax == rgb.g)
hsv.h = 85 + 43 * (rgb.b - rgb.r) / (rgbMax - rgbMin);
else
hsv.h = 171 + 43 * (rgb.r - rgb.g) / (rgbMax - rgbMin);
return hsv;
}