SUMMARY
I want to put a single https://www.sparkfun.com/products/12986 (neopixel) on my https://www.sparkfun.com/products/12587 project as a status indicator. I can’t get it to take a signal from the 3.3v Arduino Pro Micro. I tried the same code with my 5v Arduino Micro and all is well. The [Überguide says that I ought to be able to signal with 3.3v if I’m powering the neopixel with 3.7v, but that is not my experience. Any advice is appreciated.
WIRING
On the 5v board I was able to connect to D7 (with and without a 330 resistor), V5, GND, and float the data out pin to get it to work.
On the 3.3v board I’ve tried getting power from USB and the same D7 (with and without a 330 resistor), V5, GND, and float wiring but the LED stays blue.
I’ve powered the 3.3v board with a 3.7v LiPo via RAW in and D7 (with and without a 330 resistor), V5, GND, and float wiring but the LED stays blue.
I’ve powered the 3.3v board with a 3.7v LiPo via RAW in and D7 (with and without a 330 resistor), RAW, GND, and float wiring but the LED stays blue.
I’ve powered the 3.3v board with a 3.7v LiPo via VCC in and D7 (with and without a 330 resistor), V5, GND, and float wiring but the LED stays blue.
I’ve powered the 3.3v board with a 3.7v LiPo via VCC in and D7 (with and without a 330 resistor), RAW, GND, and float wiring but the LED stays blue.
CODE
#include <Adafruit_NeoPixel.h>
#define PIN            7
#define NUMPIXELS      1
Adafruit_NeoPixel pixels = Adafruit_NeoPixel(NUMPIXELS, PIN, NEO_RGB + NEO_KHZ800);
void setup() {
  Serial.begin(9600);
  pixels.begin();
  pixels.show();
  Serial.println("pixel off");
}
void loop() {
  int maxbright = 100;
  int r; int g; int b;
  for(int i=0;i<=maxbright;i+=5){
    r = maxbright-i;
    g = 0;
    b = i;
    Serial.println((String) "R:"+r+ " G:"+g+ " B:"+b);
    pixels.setPixelColor(0, pixels.Color(r,g,b));
    pixels.show();
    delay(50);
  }
}
CONCLUSION
I’ve taken the most scientific approach to this as I’m capable, but I cannot get it to work. I’m now looking for suggestions.](The Magic of NeoPixels | Adafruit NeoPixel Überguide | Adafruit Learning System)