Commonly used coordinates question for reference Station

All right so quick question regarding the rtk reference station.

In a software settings on my phone or tablet, when I create a commonly used coordinate and save it, can I save it and give it a name? If so when I call that up again and place the base station antenna at the same location and then load it will then begin broadcasting corrections like before when I set the initial base location and saved it?

Second question, can I do this without being connected to the internet so it’s just using an average or single use setup for the base?

Thank you so much for your help

Yes, I believe what you are looking for exists in the Web Config page. Please see docs here. The ‘commonly used coordinates’ allows you to enter multiple fixed base locations and switch between them depending which location are are deploying the base to that day.

Yes, you can switch without being connected to the internet. The Web Config is done over a WiFi connection between your phone and the device (device broadcasts as an access point).