I recently did 6 designs in two orders, and by and large I’m quite happy with them and the price for low quanties (I did 4 to 12 copies of each board).
My question relates to getting the board outline correct, as all of my designs were trimmed a little small. Quoting the FAQ:
This is normally done with a drawing layer, a keep out layer, or a silkscreen layer. You can use any method you want but please use one! Something as simple as a rectangle on the top overlay layer is great!
On all of my boards the back is mostly ground plane, with traces plowed through it. The ground polygon stops 0.020 from the edge of the board because I want the mask to cover the ground plane to avoid accidental shorts with the edge of the board. (Just a good standard practice.) Other services I have used will give a DRC kick-out if you take copper up to the edge, FWIW.
Anyway, to define the outline, I have a rectangle on the back silk. It is drawn with an 0.010 line, centered on the desired board outline, which is how the outline would be drawn for a fab house that wants an outline layer.
All of my boards came back trimmed to the edge of the ground polygon. In other words, whoever picked the cutting line ignored my silk rectangle and in fact whacked it off, and snapped to the edge of the copper.
All of the boards are functional this way, of course, and perfectly good as prototypes. I’d reject them as production boards, though, so Gold Phoenix wouldn’t get my production business if there wasn’t a way to correctly communicate the board outline.
In any case, I’m happy enough with the boards that I will certainly be doing more prototypes with BatchPCB, but it would be nice if I could learn to communicate the board outline in a way everybody understands. What should I do on my next design?
Thanks,
Dave