Is the “Qwiic Adapter” compatable with the “H3LIS331DL Accelerometer Breakout”?
I can use a header to connect SCL, SDA, 3.3V and GND.
Would I then connect Int1 seperatly?
If they are compatable, can i use the I2c code I currently have? or do I have to modify it with Qwiic specific code?
I am using the RedBoard Artemis Nano with the Arduino IDE. If this is possible I will also use a Qwiic button and Qwiic OLED display for this project.