Hello,
I am about to make an application using strain gages in wheatstone
configuration and I would like to ask about the modules
https://www.sparkfun.com/products/13261
https://www.sparkfun.com/products/13878
I am not using an already completed wheatstone bridge circuit (like load
cells) , but instead I am using 2 strain gages and I want to complete a
half bridge circuit configuration with these 2 gages.
My question is if any of your aforementioned modules has the ability to
complete the Wheatstone bridge ?
If yes, I will just need to wire the 2 strain gages.
If not, I will need to first find a circuit to complete the bridge and then wire the hole configuration to any of your modules. In this case is there such a bridge completion module available?
Thanks for the help,
Hi Giannis.
It’s actually super easy and you don’t need a combinator board at all. If you have two sensors, just connect them like the diagram below and you’re good to go!

Hello TS-Chris,
Thanks for the immediate response. I think your image refers to the case when load cells are used, and not strain gages which is my case. The configuration I want to make is in the image below. So I have to solder the gages in a circuit with two resistors, aren’t I ? Correct me if I 'm wrong.

Best regards,
Giannis
Hi Giannis.
Sorry about that, I thought you were referring to our [50kg Load Sensor that has a strain gauge and a resistor inside.
We don’t have a specific board or device to connect two individual stain gauges into a Wheatstone bridge, but a bit of proto board, two resistors and the leads from your strain gauges would work. Something like [PRT-12702 or [PRT-08808 is what I’d use.
Your resistors should be the same resistance as the strain gauges you’re using.](ProtoBoard - Square 1" Single Sided - PRT-08808 - SparkFun Electronics)](SparkFun Solder-able Breadboard - Mini - PRT-12702 - SparkFun Electronics)](https://www.sparkfun.com/products/10245)
Thank you.
I have been thinking of soldering the bridge completion circuit on my own but the problem is that I could not find resistor of 350 Ohm, which is the resistance of the strain gauges used.
Best regards,
Dadiotis Ioannis
You could always add several values of resistors together to get your desired value. For instance, a 330 ohm and a 20 ohm resistor connected in series will give you 350 ohms.