Hello, I am a new Spark Fun user and I have purchased a Spark Fun RTK Mosai X5 to use as a Ntrip base. I would like to know what configuration of the septentrio you recommend so as not to damage the equipment or overload it, as well as to be able to reach the greatest possible coverage distance. I would like my equipment to be able to be used as a base up to a radius of 100 km. I am sharing a configuration that I am testing. I read them and appreciate your responses.
10km is about the max radius from a base station to an on-site RTK device (‘baseline distance’) if you want 1-2cm accuracy. Farther distances are subject to the deviations in the earth’s curvature and the requisite time required for satellites to pass by
What do you mean by ‘configuration of the North’?
As for overloading…it depends on how many messages you require and how often; you can pound the bus pretty hard on the x5, but you should generally disable any extra/unnecessary messages, and anything else that requires compute resources, to free up bandwidth on the bus
Sorry, I meant septentrio, I would like to know what configuration you recommend for the transmission of RTCM messages and transmitted signals. I still haven’t been able to get the ntrip to transmit L5 and B3 signals.