Hello (this is my very first post),
I’ve been playing around with the VL53L5CX sensor and I have a use case where I will need two of these sensors connected roughly 1 meter apart.
Basically this configuration but with 50cm Qwiic cables connecting the sensors instead:
When I load the Arduino example sketch for two sensors I can see these comments:
SparkFun_VL53L5CX myImager1;
int sensorAddress1 = 0x44; //New address of unit without a wire. Valid: 0x08 <= address <= 0x77
int sensorReset1 = 14; //GPIO that is connected to the Reset pin on sensor 1
VL53L5CX_ResultsData measurementData1;
SparkFun_VL53L5CX myImager2;
int sensorAddress2 = 0x29; //Default VL53L5CX - this is the unit we'll hold in reset (has the wire soldered)
int sensorReset2 = 13; //GPIO that is connected to the Reset pin on sensor 2
VL53L5CX_ResultsData measurementData2;
But I have no idea which wires it is referring to. :? I suppose it’s the I2C traces mentioned on https://learn.sparkfun.com/tutorials/qw … e-overview?
Can someone give me some guidance on what I need to do to get this example working?
Thanks!