However, after testing it by connecting the power supply and setting the input voltage to 22 V with maximum currents at 25 A, I utilized an electronic load to draw currents from this module. The results indicate that below 10 A, it functions well; however, after setting it to a higher current (11 A), this module will cut-off circuit.
Is this a normal operation? I had expected it to consistently clamp or hold the current at 10 A (reducing the voltage instead; CC-charger) even if the load attempts to draw more current than this.
Welcome @benkingjo
That appears to be a very specialized supply, intended to recharge a 3S Li-on Pack, with a capacity over 10Ah (for a 1C rate).
Since it expects the output/load to be a 3S li-on, the current will be reduced as the load approaches 12.6V. If you try to use this as a standard 12V power supply for electronics, it will behave unexpectedly, as that is not the intended purpose.