Hi all!
I have some sound-reactive rave/festival apparel which lights up by responding to micophone output. The whole thing runs off a standard USB power brick (the type for charging phones) as I find this is the most convenient power source. This means I’m working with 5V - the WS28xx LEDs are 5V and that’s also convenient as I can run, program and debug the Teensy++ 2.0 off that same USB 5V. So, I’m sorta attached to the 5V thing.
However, the microphone is an elecrtet, and I find that in loud settings it tends to just ‘top out’ and register maximum volume all the time. I’ve tried playing the the gain, but it doesn’t seem to help much. Looking at the data sheet, I see that a typical max volume is 110dB, which would explain it, as a quick google suggests live music could easily reach 120dB.
So, I’ve decided I’d like to pick up the BOB-19389 MEMS breakout board, as it claims a max volume of over 130dB. However, I dan’t seem to find a 5V MEMS anywhere. Neither can [this guy.
So I’m looking into ways to make it compatible. I’m wondering if a simple voltage divider will work. I’ve looked up [a bunch of options, but perhaps a couple of resistors is enough. However, Dave Haynie’s answer on [this question has got me wondering.
So, given that I only really need an approximate representation of volume, and not a good quality audio signal, would a couple of resistors be enough for my purposes to take the voltage down to something that the MEMS can handle and provide me with a reading? If so, can you recommend some resistor values? I’m trying to balance power usage with making sure the MEMS has enough power to do its thing.](https://www.quora.com/How-do-I-convert-a-5-V-DC-to-3-3-V-DC-using-resistors-voltage-divider-I-have-a-couple-of-220-Ω-560-Ω-2-2-kΩ-and-10-kΩ-resistors)](Taking It To Another Level: Making 3.3V Speak With 5V | Hackaday)](5V mems mic breakout - SparkFun Electronics Forum)