Hi everyone,
I have a Copernicus DIP II (https://www.sparkfun.com/products/11858) with the SMA antenna (https://www.sparkfun.com/products/177). Using the following setup:
Vcc → 3.3V
GND → 0V
XSTBY → Vcc
Im powering up the GPS using an external power supply.
I am able to communicate the GPS, and I have already set it up to receive and return messages in TAIP protocol. Also, I’m able to get the time but I cannot get a fix. I have been testing the GPS using Trimble GPS Studio.
Tests:
Command: >QTM;*67<
Return Message: >RTM0329448390211201416900100000;*64<
This command return the time, which is correct (when I sent the command). But the last 9 states that is without a fix.
The real problem is when I try to get coordinates:
Command: >QCP;*6D<
Return Message: >RCP00000+000000+000000091;*66<
This command is all wrong. It returns all 0, without a fix.
I was wondering if someone encounter this problem before? How to fix this?