As the title suggests I’m looking to see if the Myoware could be used as a chest heart rate monitor. I’m looking to build a chest hr monitor for my capstone and was wondering if I could use this. The monitor I’m looking to build is going to be used during physical activity, so I want it to be pretty compact and not have wires going every which way, like some ECGs that also monitor the orientation of the heart. Any help is greatly appreciated!
Not readily, but we do sell SparkFun Single Lead Heart Rate Monitor - AD8232 - SEN-12650 - SparkFun Electronics