CRC Check Failed with ORPSoC system

Hello there,

Reference: http://kevinmehall.net/openrisc/guide/

I m a newbie to ORPSoC and OpenOCD, and i ve been trying to build an OrpSoC system based on the tutorial provided with the reference. Once the system is build and the OpenOCD is triggered, it throws in an error

jeebu@jeebu:~/openrisc/toolchain/openOCD$ sudo ./src/openocd -f ./tcl/interface/altera-usb-blaster.cfg -f altera-dev.tcl

Open On-Chip Debugger 0.5.0-dev-g187f984 (2014-04-30-19:46)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.berlios.de/doc/doxygen/bugs.html

Info : only one transport option; autoselect ‘jtag’

3000 kHz

Warn : Interface already configured, ignoring

3000 kHz

Info : No lowlevel driver configured, will try them all

Info : usb blaster interface using libftdi

Info : clock speed 3000 kHz

Info : JTAG tap: or1k.cpu tap/device found: 0x020f30dd (mfg: 0x06e, part: 0x20f3, ver: 0x0)

Warn : JTAG tap: or1k.cpu UNEXPECTED: 0x020f30dd (mfg: 0x06e, part: 0x20f3, ver: 0x0)

Error: JTAG tap: or1k.cpu expected 1 of 1: 0x020b30dd (mfg: 0x06e, part: 0x20b3, ver: 0x0)

Error: Trying to use configured scan chain anyway…

Warn : Bypassing JTAG setup events due to errors

Error: received CRC (0xfff927ff) not same as calculated CRC (0x2926cf53)

Error: received CRC (0x496db27f) not same as calculated CRC (0x6d09534e)

Error: received CRC (0xfff927ff) not same as calculated CRC (0x2926cf53)

Error: received CRC (0x496db27f) not same as calculated CRC (0x6d09534e)

Warn : Debug IF CPU control reg read failure.

Warn : Resetting JTAG TAP state and reconnectiong to debug IF.

Warn : attempt 1 of 5

Error: received CRC (0xfff927ff) not same as calculated CRC (0x2926cf53)

Error: received CRC (0x496db27f) not same as calculated CRC (0x6d09534e)

Warn : Debug IF CPU control reg read failure.

Warn : Resetting JTAG TAP state and reconnectiong to debug IF.

I m unable to solve this issue of CRC. Need some help.

Regards

Jeebu Jacob Thomas