I have been trying to run openocd using a parallel port. So far I had small success.
First, I am using the version 0.4.0 of OpenOCD.
I downloaded and configured using:
./configure --enable-parport
make
make install
Next, I used the following configuration files:
paralela.cfg
#daemon configuration
telnet_port 4444
gdb_port 3333
#interface
interface parport
parport_port 0x378
parport_cable wiggler
and then, Lm3s811.cfg which came with OpenOCD v0.2.0
# Script for luminary lm3s811
if { [info exists CHIPNAME] } {
set _CHIPNAME $CHIPNAME
} else {
set _CHIPNAME lm3s811
}
if { [info exists ENDIAN] } {
set _ENDIAN $ENDIAN
} else {
# this defaults to a little endian
set _ENDIAN little
}
if { [info exists CPUTAPID ] } {
set _CPUTAPID $CPUTAPID
} else {
# force an error till we get a good number
set _CPUTAPID 0x3ba00477
}
# jtag speed
jtag_khz 1
jtag_nsrst_delay 100
jtag_ntrst_delay 100
#LM3S811 Evaluation Board has only srst
reset_config srst_only
#jtag scan chain
jtag newtap $_CHIPNAME cpu -irlen 4 -ircapture 1 -irmask 0xf -expected-id $_CPUTAPID
# the luminary variant causes a software reset rather than asserting SRST
# this stops the debug registers from being cleared
# this will be fixed in later revisions of silicon
set _TARGETNAME [format "%s.cpu" $_CHIPNAME]
target create $_TARGETNAME cortex_m3 -endian $_ENDIAN -chain-position $_TARGETNAME -variant lm3s
# 8k working area at base of ram
$_TARGETNAME configure -work-area-virt 0 -work-area-phys 0x20000000 -work-area-size 0x2000 -work-area-backup 0
Then, following error comes when I use
openocd -f paralela.cfg -f lm3s811.cfg
Error: JTAG scan chain interrogation failed: all ones
Error: Check JTAG interface, timings, target power, etc.
Can someone please help me!
Thanks!