CS-E9032 Linux 2.6 kernel build problem

Hi all!

I used the CS-E9302(Debian) native gcc to compile linux-2.6.24-rc8 at the “LD .tmp_vmlinux1” state, the following error occured:

/bin/sh: line 1:  9391 Killed                  ld -EL -p --no-undefined -X -o .tmp_vmlinux1 -T arch/arm/kernel/vmlinux.lds arch/arm/kernel/head.o arch/arm/kernel/init_task.o init/built-in.o --start-group usr/built-in.o arch/arm/kernel/built-in.o arch/arm/mm/built-in.o arch/arm/common/built-in.o arch/arm/mach-ep93xx/built-in.o arch/arm/nwfpe/built-in.o kernel/built-in.o mm/built-in.o fs/built-in.o ipc/built-in.o security/built-in.o crypto/built-in.o block/built-in.o arch/arm/lib/lib.a lib/lib.a arch/arm/lib/built-in.o lib/built-in.o drivers/built-in.o sound/built-in.o net/built-in.o --end-group
make: *** [.tmp_vmlinux1] Error 137

My gcc version is :

gcc (GCC) 4.1.2 20061115 (prerelease) (Debian 4.1.1-21)
Copyright (C) 2006 Free Software Foundation, Inc.
This is free software; see the source for copying conditions.  There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

My gcc has problem ???

Thank you.

Oh no, my gcc worked OK!

My memory may be exhausted.

I found it when using the “free -m” command line.

temporally, I created a 256MB swap file, and build the linux 2.6 kernel again.

Hope it works without problem!