I have compiled linux kernel 2.6.19 and everything looks good. Kernel started and send standard msgs to serial port but kernel panic during attempt to mount root fs. Standard included to CS_E9301 board ram disk image is loaded to ram (0x00800000). But kernel can’t recognize it and mount as a root partition. In configuration file (ep93xxxx_defconfig) I got
CONFIG_BLK_DEV_RAM=y
CONFIG_BLK_DEV_RAM_SIZE=16384
CONFIG_BLK_DEV_INITRD=y
NOTE: I don’t see messages about RAMDISK in my kernel ouput, during execute 2.6.8 kernel delivered by olimex RAMDISK messages exists.
Kernel boot output:
RedBoot> Uncompressing Linux…
… done, booting
the kernel.
Linux version 2.6.19.6 (root@goolbiiLx) (gcc version 4.1.1) #6 T
hu Jun 14 11:53:27 CEST 2007
CPU: ARM920T [41129200] revision 0 (ARMv4T), cr=c0007177
Machine: Olimex CS-E9301
Memory policy: ECC disabled, Data cache writeback
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 64, 32 byte lines, 8 s
ets
CPU0: D cache: 16384 bytes, associativity 64, 32 byte lines, 8 s
ets
Built 1 zonelists. Total pages: 8016
Kernel command line: console=ttyAM root=/dev/ram
PID hash table entries: 128 (order: 7, 512 bytes)
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 8MB 8MB 8MB 8MB = 32MB total
Memory: 29704KB available (2224K code, 433K data, 84K init)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
ep93xx: PLL1 running at 331 MHz, PLL2 at 192 MHz
ep93xx: FCLK 165 MHz, HCLK 66 MHz, PCLK 33 MHz
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
NET: Registered protocol family 2
IP route cache hash table entries: 256 (order: -2, 1024 bytes)
TCP established hash table entries: 1024 (order: 2, 16384 bytes)
TCP bind hash table entries: 512 (order: 1, 10240 bytes)
TCP: Hash tables configured (established 1024 bind 512)
TCP reno registered
NetWinder Floating Point Emulator V0.97 (extended precision)
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
io scheduler noop registered
io scheduler deadline registered (default)
ep93xx_wdt: EP93XX watchdog, driver version 0.3 (nCS1 disable de
tected)
Serial: AMBA driver $Revision: 1.41 $
apb:uart1: ttyAM0 at MMIO 0x808c0000 (irq = 52) is a AMBA
apb:uart2: ttyAM1 at MMIO 0x808d0000 (irq = 54) is a AMBA
apb:uart3: ttyAM2 at MMIO 0x808e0000 (irq = 55) is a AMBA
physmap platform flash device: 01000000 at 60000000
physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank
Intel/Sharp Extended Query Table at 0x0031
Using buffer write method
cfi_cmdset_0001: Erase suspend on write enabled
cmdlinepart partition parsing not available
Searching for RedBoot partition table in physmap-flash.0 at offs
et 0xfe0000
7 RedBoot partitions found on MTD device physmap-flash.0
Creating 7 MTD partitions on “physmap-flash.0”:
0x00000000-0x00040000 : “RedBoot”
0x00040000-0x00540000 : “netbsd”
0x00540000-0x00a40000 : “netbsd_install”
0x00a40000-0x00d40000 : “ramdisk.gz”
0x00d40000-0x00e20000 : “zImage”
0x00fc0000-0x00fc1000 : “RedBoot config”
mtd: partition “RedBoot config” doesn’t end on an erase block –
force read-only
0x00fe0000-0x01000000 : “FIS directory”
ep93xx-ohci ep93xx-ohci: EP93xx OHCI
ep93xx-ohci ep93xx-ohci: new USB bus registered, assigned bus nu
mber 1
ep93xx-ohci ep93xx-ohci: irq 56, io mem 0x80020000
usb usb1: Product: EP93xx OHCI
usb usb1: Manufacturer: Linux 2.6.19.6 ohci_hcd
usb usb1: SerialNumber: ep93xx
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 3 ports detected
Initializing USB Mass Storage driver…
usb 1-3: new full speed USB device using ep93xx-ohci and address
2
usb 1-3: Product: USB 2.0(FS) FLASH DISK
usb 1-3: SerialNumber: USB 2.0(FS) FLASH DISK
usb 1-3: configuration #1 chosen from 1 choice
scsi0 : SCSI emulation for USB Mass Storage devices
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
drivers/usb/net/rtl8150.c: rtl8150 based usb-ethernet driver v0.
6.2 (2004/08/27)
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver usbserial
drivers/usb/serial/usb-serial.c: USB Serial Driver core
drivers/usb/serial/usb-serial.c: USB Serial support registered f
or pl2303
usbcore: registered new interface driver pl2303
drivers/usb/serial/pl2303.c: Prolific PL2303 USB to serial adapt
or driver
ep93xx-rtc ep93xx-rtc: rtc intf: sysfs
ep93xx-rtc ep93xx-rtc: rtc intf: proc
ep93xx-rtc ep93xx-rtc: rtc intf: dev (254:0)
ep93xx-rtc ep93xx-rtc: rtc core: registered ep93xx as rtc0
i2c /dev entries driver
TCP cubic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
NET: Registered protocol family 15
ep93xx-rtc ep93xx-rtc: setting the system clock to 1970-01-01 08
:25:02 (30302)
VFS: Cannot open root device “ram” or unknown-block(1,0)
Please append a correct “root=” boot option
Kernel panic - not syncing: VFS: Unable to mount root fs on unkn
own-block(1,0)
![]()
Regards Michal