I’m a software engineer by trade, but don’t know much about micro electronics, so I apologize in advance for my ignorance. I’m trying to pull together a hobby project and was hoping you guys might be able to point me in the right direction.
The project in question involves a portable UV water purification system. There is a 12 volt, 4 amp battery (charged via solar panel) that is connected through a standard commercial inverter to power a 110 volt 13 watt UV sterilization lamp.
What I’m trying to figure out is how to integrate a component that monitors the power being drawn by the lamp to operate a solenoid valve that shuts off the flow of water until the lamp is fully “warmed up” so that I can prevent water running until sterilization is happening…
In short, I think what I need is some kind of circuit that monitors the current between the inverter and the UV lamp and then trips a relay to energize the solenoid on the valve once the lamp is drawing full power so that water can flow.
There is a PDF describing the project, in general terms, here: http://www.simpleearthstructures.com/re … atment.pdf
I was wondering if you could tell me if there are any pre-made components that I might purchase that would work for this application or if you know of a way that I can pay someone to either draw up plans or manufacture a few of these circuits for me? The PDF made it sound like it was easy to do, but I have no idea.
Thanks so much in advance! Your time and information is greatly appreciated!