Dead Reckoning GPS and logging

I need to log data from a dead reckoning GPS and other sensors. I have the SparkFun GPS Dead Reckoning Breakout - NEO-M8U (Qwiic) and the SparkFun DataLogger IoT boards. The M8U isn’t listed a directly supported by the Data logger board but is there a way to bring in the GPS dead reckoning data so that it is synced with the data from the other sensor boards?

Hi,

The DataLogger IoT is able to log data from the NEO-M8U, but only Position-Velocity-Time data (Latitude, Longitude, Heading, etc.). There is currently no way to make it log (e.g.) the vehicle attitude.

I hope this helps,

Paul

I am looking to use the dead reckoning feature to log position in a tunnel. Will the “dead reckoning determined position” be calculated on the NEO-M8U and sent to the logger as longitude/latitude?

The Data logger IoT board has an IMU - can I get attitude data logged from this source? If so, would I need to align the orientation of the data logger board and the NEO-M8U board?

Hi,

The dead reckoning capability will certainly help inside a tunnel. And, yes, the latitude/longitude will be updated based on the NEO’s internal IMU.

The DataLogger IoT 9-DOF has on-board IMU (Accelerometer and Gyro) and Magnetometer. You can calculate “AHRS” attitude from that. The sensor axes are marked on the PCB - both on the 9-DOF and NEO.

Best wishes,

Paul

Thank you!