I use the Sparkfun PIC development boards (PIC-P8, PIC-P14, PIC-P18, etc) for prototyping my projects. I use wire-wrap as well. These boards are nice for this except for one thing; the holes are just a little too small. The standard wire wrap pins require a 0.042" hole and these boards appear to have about 0.039" holes (at least as I have been able to measure). They are just a little too small to be able to press fit the wire wrap pins.
It would really be nice if these boards were made with 0.042" holes.
Mike