Digimesh 900MHz units in transparent mode: do they all recieve the same data from a transmitter?

Hi all,

Does anyone know if, for example, 3 modules set in ‘transparent mode’ in a Digimesh network will all send out the same data from a single transmitter. For example: There are 3 units #1, #2 and #3 with unit #2 in the middle of units #1 and #3. Unit #3 is out of direct range with Unit#1 - so all data is routed via Unit #2. Unit #1 transmits some data onto the Digimesh network. Is it the case that units #2 and #3 will both receive the data (and send out each of their respective serial ports)?

Thanks,

David.