Disassembly not working

Hello

I’m using an lpc210x/lpc23xx and openocd reports me in the help

the disassembly command. But wenn i call it

via disassembly 0x1234 8, it says:

disassemble 0x1234 4

Command disassemble not found

The config says

…

target arm7tdmi little reset_run 0 arm7tdmi-s_r4

…

Thanks

The ‘disassemble’ command belongs to the ‘armv4_5’ group of commands:

armv4_5    armv4/5 specific commands
               reg -    display ARM core registers
        core_state -    display/change ARM core state <arm|thumb>
       disassemble -    disassemble instructions <address> <count> ['thumb']

The correct command line is “armv4_5 disassemble 0x1234 4”.

Other command groups are ‘flash’, ‘arm7_9’, …

Regards,

Dominic