Bought three Sparkfun BOB-09816 op-amp breakout boards for use in a noise detection project.
I am having a problem getting them to correctly amplify signals below about 80Hz.
With an input of a 1 volt peak to peak sine wave and the board’s potentiometer set so that the output of the board does not saturate, I get distortion at the positive and negative peaks as the signal frequency is reduced from 100Hz down to 50Hz. The distortion kicks in at around 80Hz. Above 100Hz, they behave as expected.
Any help would be appreciated.