DIY an FPGA development board, beginner

Hello. I have an Spartan 3 xc3s400 4tqg144c FPGA. I want to build a FPGA development board for education undergraduate university. Which components do i need to buy? I am a beginner. Thank you.

I’m afraid this is not a beginner project. You would be much better off purchasing a ready made FPGA development board.

Useful information about development boards here: https://www.raypcb.com/xilinx-spartan-3/

It will be obvious why building one is not a DIY project.

YellowDog:
I’m afraid this is not a beginner project. You would be much better off purchasing a ready made FPGA development board.

Thank you so much . I searched and found that i need components like these but I'm worry for compatibility. Is it ok to order below list?

IS62LV256AL-20TLI

TSOPI-28-8.0mm SRAM ROHS

FT2232HL-REEL

-40℃~+85℃ UART LQFP-64(10x10) USB ICs ROHS

M25P40

SO-8 NOR FLASH ROHS

ASDM1-50.000MHZ-LC-T

LVCMOS -40℃~+85℃ 3.3V~3.3V 50MHz 10mA SMD2520-4P Oscillators ROHS

ADP7182AUJZ-2.5-R7

LDO Voltage Regulators -30V, 200mA, low noise, Linear Reg, 2.5V

LT1963ES8-3.3

SO-8 Linear Voltage Regulators (LDO) ROHS

SSP1117-1.2V

1A 1.5V@(1A) Fixed 1.2V~1.2V Positive 1 20V SOT-223 Linear Voltage Regulators (LDO) ROHS

X2001WR-2x08A-6TV01

  • IDC Connectors

jremington:
Useful information about development boards here: https://www.raypcb.com/xilinx-spartan-3/

It will be obvious why building one is not a DIY project.

Thank you. The page is so useful.

You’re free to order whatever you wish but I still think you would be better off ordering a ready made board.

A DIY attempt to make an FPGA development board will certainly be a learning experience.

YellowDog:
You’re free to order whatever you wish but I still think you would be better off ordering a ready made board.

Thank you Sir.

jremington:
A DIY attempt to make an FPGA development board will certainly be a learning experience.

Thank you Sir

Thank you all. I have just a XC3S400-4TQG144C chip and I searched and found that i need at least theses components:

-a Configuration Memory Flash PROM, for example XCF04S

-an High speed asynchronous SRAM 256 kbit, give me an example??

-An EEPROM like AT24C08

-an oscillator

The problem is, which compatible components list should i order?