Has anybody gotten the SparkFun DMX Example 2 Input program to work with a SparkFun ESP32-S2 Thing Plus and the SparkFun DMX Shield?
I changed the enable pin to GPIO 3 to match the development board, the program compiles and loads, showing that it thinks DMX was initialized. And I can see that it is getting DMX to the 33/RX1 pin with my scope. But it never shows that anything was received.
I suspect the problem is that the DMX receiving port isn’t being correctly created. The program does this with the “HardwareSerial dmxSerial(2);” statement. I tried changing it to dmxSerial(1), and replacing “dmxSerial” with “Serial1”, but neither helped.
No wiring to show. Just a SparkFun Thing Plus - ESP32-S2 WROOM (WRL-17743) plugged into a SparkFun ESP32 Thing Plus DMX to LED Shield (DEV-15110).
Library is SparkFun DMX Shield Library 2.0.1. Program is the Example 2 - DMX Input from that library, with the only change setting enPin to 3 instead of 21.
As I said, the DMX shield is properly delivering DMX to pin 14 of J4 on the ESP32-S2 Thing Plus (33/RX1).
Ok; usually these fellas have wiring/cables…it really helps to post those so the people who are responding/trying to help are not making wiring/soldering assumptions :-/
I do see your original intent was to see if someone had gotten example 2 work, so I’ll hang tight while we await such
Or maybe look at the example that SparkFun provided with the library. I expect that the problem is with the statement “HardwareSerial dmxSerial(2);” which seems to be an anacronism from the original ESP32 which had three UARTs.
Ok I looked at it. With that in mind I still think example 2 requires 2 MCUs (thing pluses, I believe you have 2) and 2 DMX shields (I believe you have one?) wired as detailed in the example 2 section of the hookup guide SparkFun ESP32 DMX to LED Shield - SparkFun Learn; do you have 2 DMX shields?
The problem is with specifying the serial port to use. The examples do that with:
HardwareSerial dmxSerial(2);
That probably worked on the original ESP32, which had three UARTs, but the ESP32-S2 has only two. I tried changing it to dmxSerial(1) but that didn’t seem to work.
Yes, with the ESP32-S2. With the ESP32-C6, there seems to be a problem with the break detection, such that sometimes the DMX slots are shifted. DMX is a problem because it depends on handling the break detection to have things synchronized, that’s not well supported in Arduino serial libraries.
Also, for the C6, use Serial0 instead of Serial1 and gpio9 instead of gpio3 for the read enable.