I’ve made a design, and after making a board from it I have come to the point where the layout is where I want it except the PIN23 GND has no connection to ground. PIN3 GND still has connection as normal. I have tried starting again, but end up with more problems so Im thinking I may just remove that pin from ground.
Thanks Leon, managed to sort it with some re-jiggery. A problem Im having is trying to implement a LM2576 and the design is passing DRC now with exception to all the pads of the 2576 being merged together. It looks fine in the editor, I have even tried reducing the pad size but it still merges them in the board layout.
Hi, I managed to sort it by moving the pads 0.0125 apart, I may have to bend the leads but I now get no DRC errors. I will take a screenshot and upload the library when I get home.