Hello ,
Some Days ago i had get neo-m8p .
I see that the Led Fancing blinking as pps led if I power the bord from one side and enable ever if powered from another side .
I solder a Strip into pin for maximum 3 seconds at 260 ° .
In your opinion the Breadborad is domage or not ? … it is Very expensive …
I see that the U-Center connect correctly to Module and I received messages in NEMEA FORMAT with no problem .
If by u- center i set Fancing parameter the LED everithing blink but the message in UBX retur the correct information … it is very strange .
In your opinion are there electrical problem ? or in your component the result is the same ?
Many thank fo your opinion and Reply .